8536IB1904EN-04

Safety-Related Sensor Element

The SIM module is connected upstream:

  • to the 24 Vdc source

  • to the safety-related sensor element or a Preventa XPS module (or equivalent).

The SIM module is designed with two input channels to accommodate dual channel safety-related sensor elements. For a higher level of fault tolerance, the two-input channel architecture is recommended.

For the wiring diagrams below, refer to Legend for SIM Channel Wiring Diagrams.

SIM — One Channel Wiring

SIM — Two Channel Wiring

Legend for SIM Channel Wiring Diagrams

Emergency stop push button (S1)

Flat cable connector

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.