8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 3/4 Configuration

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 3/4 according to ISO 13849. Stop Category 0 according to EN/IEC 60204–1.

The SIL Stop of the motor is directly controlled by the opening of the contact of the emergency stop push button.

SIL Stop, Wiring Category 3/4

Avatar A1

Bus coupler

SIL Group 1

24 VDC

Motor

Preventa XPS-UAF Module

Wiring Category 3/4, Stop Category 0

PLC

Example: Motor One Direction - SIL Stop, W. Cat 3/4 — Stop Category 0, Wiring Category 3/4 Configuration

Legend for Example: Motor One Direction - SIL Stop, W. Cat 3/4 — Stop Category 0, Wiring Category 3/4 Configuration

Power supply

Start button (S2)

Emergency stop push button (S1)

Input

Flat cable connector

Start

SIL interface module (SIM)

Extension

Preventa XPS-UAF Module

   
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.