8536IB1904EN-04

Installation Tests

Perform the steps in the following table to test the installation of the safety function.

Installation Test

1

Using the DIAGNOSTICS panel in the TeSys™ island DTM, verify that the physical topology matches the logical topology.

2

Using the MY AVATAR panel in the TeSys island DTM, verify in AVATAR PARAMETERS that the SIL* avatars are associated with the proper SIL group.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.