8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 2 Configuration

NOTE: Safety Integrity Level according to standard IEC 61508. Wiring Category 2 according to ISO 13849. Stop Category 0 according to EN/IEC 60204-1.

Example: Motor Two Directions - SIL Stop, W. Cat 1/2 — Stop Category 0, Wiring Category 2 Configuration (Indirect Monitoring)

Legend for Example: Motor Two Directions - SIL Stop, W. Cat 1/2 — Stop Category 0, Wiring Category 2 Configuration (Indirect Monitoring)

Mechanical interlock

Bus coupler

Parallel link

PLC

Reversing link

Upstream circuit breaker

Emergency stop push button (S1)

Power supply

Flat cable connector

Input

SIL interface module (SIM)

Start

Preventa XPS-UAF Module

Extension

Start button (S2)

   

Example: Motor Two Directions - SIL Stop, W. Cat 1/2 — Stop Category 0, Wiring Category 2 Configuration (Direct Monitoring)

Mechanical interlock

SIL interface module (SIM)

Parallel link

Safety Function PLC

Reversing link

Upstream circuit breaker

Emergency stop push button (S1)

Digital input

Flat cable connector

Digital output

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.