8536IB1904EN-04

SIL Stop, Stop Category 0, Wiring Category 1

Example: SIL Stop, Stop Category 0, Wiring Category 1 *

Mechanical interlock

Emergency stop push button (S1)

Parallel link

Flat cable connector

Reversing link

SIL interface module (SIM)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.