8536IB1904EN-04

Wiring Category 1

A single detected fault may lead to the loss of the safety function and no diagnostic coverage is required.

The safety-related sensor element can be directly wired to the SIL-IN/SIL Common inputs.* The Mirror In/Mirror Out inputs are not used. For more information on wiring the SIL-IN/SIL Common inputs, see Safety-Related Sensor Element.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.