8536IB1904EN-04

Device Usage Checks

Perform the checks described in the following table to verify that the SIL* starter contactor cycles are within the acceptable lifetime values.

1

Using the Devices DIAGNOTSICS feature of the TeSys™ island DTM or OMT, access the device asset information for each SIL starter.

2

If the Number of Contactor Cycle is greater than B10d (=1,369,863), then replace the SIL starter.

3

If not, use the Number of Contactor Cycle value to schedule the next maintenance. See Maintenance Schedule.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.