8536IB1904EN-04

High Switching Frequency (≥ 15 cycles per hour)

Updated D1

For high frequency use, the safety function must be isolated from the operational function by using a SIL* avatar for the safety function and a standard avatar for the operational function. The standard starters are then wired in series downstream the SIL starter(s). High Switching Frequency – Operational and Safety Functions table shows examples of standard avatars used downstream the SIL starter(s) for SIL Stop, W. Cat 1/2* and SIL Stop, W. Cat 3/4* architectures.

Standard Avatar for Operational Function + SIL Avatar Used for Safety Function —SIL Stop, W. Cat 1/2

Standard avatar

SIL avatar

High Switching Frequency - SIL Stop, W. Cat 1/2 — Operational and Safety Functions

Standard Avatar

SIL Avatar

Module 1

Module 2

Module 3

Module 4

Module 5

Module 6

Switch

Switch - SIL Stop, W. Cat 1/2

Standard Starter

SIL Starter

SIM

Motor One Direction

Switch - SIL Stop, W. Cat 1/2

Standard Starter

SIL Starter

SIM

Motor Two Directions

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

SIL Starter

SIM

Motor Two Speeds

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

SIL Starter

SIM

Motor Two Speeds Two Directions

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIM

Conveyor One Direction

Switch - SIL Stop, W. Cat 1/2

Standard Starter

SIL Starter

SIM

Conveyor Two Directions

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

SIL Starter

SIM

Motor Y/D One Direction

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIM

Motor Y/D Two Directions

Switch - SIL Stop, W. Cat 1/2

Standard Starter

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIM

Standard Avatar for Operational Function + SIL Avatar Used for Safety Function — SIL Stop, W. Cat 3/4

Standard avatar

SIL avatar

High Switching Frequency - SIL Stop, W. Cat 3/4 — Operational and Safety Functions

Standard Avatar SIL Avatar Module 1 Module 2 Module 3 Module 4 Module 5 Module 6 Module 7

Switch

Switch - SIL Stop, W. Cat 3/4

Standard Starter

SIL Starter

SIL Starter

SIM

Motor One Direction

Switch - SIL Stop, W. Cat 3/4

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Two Directions

Switch - SIL Stop, W. Cat 3/4

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Two Speeds

Switch - SIL Stop, W. Cat 3/4

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Two Speeds Two Directions

Switch - SIL Stop, W. Cat 3/4

Standard Starter

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Y/D One Direction

Switch - SIL Stop, W. Cat 3/4

Standard Starter

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Motor Y/D Two Directions

Switch - SIL Stop, W. Cat 3/4

Standard Starter

Standard Starter

Standard Starter

Standard Starter

SIL Starter

SIL Starter

SIM

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.