8536IB1904EN-04

SIL Starters

WARNING
UNINTENDED EQUIPMENT OPERATION
For complete instructions about functional safety, refer to the TeSys™ island Functional Safety Guide, 8536IB1904.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

SIL* starters provide similar functions to standard starters but are associated with a SIL interface module.

The main functions of the SIL starters are as follows:

  • Provide Stop Category 0 and Stop Category 1* functionality

  • Provide operational control for loads

  • Measure electrical data related to the load

  • Provide energy monitoring data when a voltage interface module is installed in the TeSys island

Multiple SIL starters might be needed for a single TeSys avatar function. For example, the avatar Motor Two Directions - SIL Stop, W. Cat 1/2* includes two SIL starters. In addition, avatars using SIL starters always include a SIL interface module.

The SIL starters are connected:

  • Upstream to a circuit breaker

  • Downstream to the load

The SIL starters communicate with the bus coupler, sending operational data and receiving commands.

SIL Starter Ratings

Power Ratings

Amperage

Reference

kW

hp

4

5

0.18–9

TPRSS009

11

15

0.5–25

TPRSS025

18.5

20

0.76–38

TPRSS038

30

40

3.25–65

TPRSS065

37

40

4–80

TPRSS080

SIL Starter Features

Flat cable (for connection with the module to the left)

Name tag

LED status indicators

Mobile bridge

Upstream power connections

Downstream power connections

QR code

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.