Block Output
The table lists the block output for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0ED6 |
3799 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0ED7 |
3800 |
1 |
0x03, |
RW |
0.01 |
s |
UINT16 |
0–60000 |
0 |
Y |
Contactor or Breaker open time |
|
0x0ED8 |
3801 |
2 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |