Temperature Protection
The table lists the temperature protection for the LTMT main unit.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0ECD |
3790 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
0x0ECE |
3791 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
°C |
UINT16 |
250–1800 |
1300 |
Y |
PT100 pickup* |
F |
770-3560 |
||||||||||
0x0ECF |
3792 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
Ω |
UINT16 |
2700–4000 |
2700 |
Y |
PTC pickup |
0x0ED0 |
3793 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
Ω |
UINT16 |
1600–2300 |
1600 |
Y |
PTC pickup reset |
0x0ED1 |
3794 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
10 |
Y |
Time delay |
0x0ED2 |
3795 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
°C |
UINT16 |
250–1800 |
1300 |
Y |
PT100 alarm level* |
F |
770-3560 |
||||||||||
0x0ED3 |
3796 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0ED4 |
3797 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
– |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0ED5 |
3798 |
1 |
0x03, 0x06, 0x10 |
RW |
0 |
– |
UINT16 |
– |
– |
– |
Reserved |