Motor Run Indicators
The table lists the motor run indicators for the Modbus RTU communication.
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
---|---|---|---|---|---|---|
0x0210 |
529 |
0x02 |
R |
BOOL | N |
Motor forward running |
0x0211 |
530 |
0x02 |
R |
BOOL | N |
Motor reverse running |
0x0212 |
531 |
0x02 |
R |
BOOL | N |
Motor fast forward running |
0x0213 |
532 |
0x02 |
R |
BOOL | N |
Motor fast reverse running |
0x0214 |
533 |
0x02 |
R |
BOOL | N |
Motor running in star (forward) |
0x0215 |
534 |
0x02 |
R |
BOOL | N |
Motor running in delta (forward) |
0x0216 |
535 |
0x02 |
R |
BOOL | N |
Motor running in star (reverse) |
0x0217 |
536 |
0x02 |
R |
BOOL | N |
Motor running in delta (reverse) |
0x0218 |
537 |
0x02 |
R |
BOOL | N |
Motor in star-delta changeover (forward) |
0x0219 |
538 |
0x02 |
R |
BOOL | N |
Motor in star-delta changeover (reverse) |
0x021A |
539 |
0x02 |
R |
BOOL | N |
Interlocking time active |
0x021B |
540 |
0x02 |
R |
BOOL | N |
Change-over pause active |
0x021C–0x021F |
541–544 |
– |
– |
– |
– |
Reserved |