Voltage Phase Reversal Protection
The table lists the voltage phase reversal protection for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0E44 |
3653 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
0x0E45 |
3654 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
0x0E46 |
3655 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0E47 |
3656 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0E48 |
3657 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |