DOCA0355EN-00

Motor Status

The table lists the motor status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x00F0

241

0x02

R

BOOL N

Motor Stop

0x00F1

242

0x02

R

BOOL N

Motor Start

0x00F2

243

0x02

R

BOOL N

Motor Run

0x00F3

244

0x02

R

BOOL N

Motor Inhibit

0x00F4 245

0x02

R

BOOL N Remote Mode

0x00F5–0x00FF

246–256

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?