DOCA0355EN-00

Common Trip, Alarm, and Pickup Status

The table lists the common trip, alarm and pickup status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x00E0

225

0x02

R

BOOL N

Pickup status

0x00E1

226

0x02

R

BOOL N

Alarm status

0x00E2

227

0x02

R

BOOL N

Trip status

0x00E3

228

0x02

R

BOOL N

Motor stop error detection

0x00E4

229

Reserved

0x00E5

230

0x02

R

BOOL N

Block output

0x00E6–0x00EF

231–240

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?