DOCA0355EN-00

Under Power Factor Protection

The table lists the under power factor protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E65

3686

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0E66

3687

1

0x03,
0x06,
0x10

RW

0.10

PF

UINT16

40–100
(step 1)

60

Y

Pickup

0x0E67

3688

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0E68

3689

1

0x03,
0x06,
0x10

RW

0.10

PF

UINT16

40–100
(step 1)

60

Y

Alarm level

0x0E69

3690

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset Key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E6A

3691

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E6B

3692

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?