DOCA0355EN-00

Permissive Commands Status

The table lists the permissive commands status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0220

545

0x02

R

BOOL N

Status - Permissive Command 1

0x0221

546

0x02

R

BOOL N

Status - Permissive Command 2

0x0222

547

0x02

R

BOOL N

Status - Permissive Command 3

0x0223

548

0x02

R

BOOL N

Status - Permissive Command 4

0x0224

549

0x02

R

BOOL N

Status - Permissive Command 5

0x0225

550

0x02

R

BOOL N

Status - Permissive Command 6

0x0226

551

0x02

R

BOOL N

Status - Permissive Command 7

0x0227

552

0x02

R

BOOL N

Status - Permissive Command 8

0x0228–0x023F

553–576

Reserved
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?