DOCA0355EN-00

Inhibit Status

The table lists the inhibit status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0240

577

0x02

R

BOOL N

No voltage inhibit

0x0241

578

0x02

R

BOOL N

Under voltage inhibit

0x0242

579

0x02

R

BOOL N

Trip inhibit

0x0243

580

0x02

R

BOOL N

Thermal inhibit

0x0244

581

0x02

R

BOOL N

Max starts inhibit

0x0245

582

0x02

R

BOOL N

Interlock 1 inhibit

0x0246

583

0x02

R

BOOL N

Interlock 2 inhibit

0x0247

584

0x02

R

BOOL N

Interlock 3 inhibit

0x0248

585

0x02

R

BOOL N

Interlock 4 inhibit

0x0249

586

0x02

R

BOOL N

Interlock 5 inhibit

0x024A

587

0x02

R

BOOL N

Interlock 6 inhibit

0x024B

588

0x02

R

BOOL N

Interlock 7 inhibit

0x024C

589

0x02

R

BOOL N

Interlock 8 inhibit

0x024D

590

0x02

R

BOOL N

Interlock 9 inhibit

0x024E

591

0x02

R

BOOL N

Interlock 10 inhibit

0x024F

592

0x02

R

BOOL N

Interlock 11 inhibit

0x0250

593

0x02

R

BOOL N

Interlock 12 inhibit

0x0251

594

0x02

R

BOOL N

Local DI stop inhibit

0x0252

595

0x02

R

BOOL N

Remote DI stop inhibit

0x0253

596

0x02

R

BOOL N

Communication stop inhibit

0x0254

597

0x02

R

BOOL N

Force stop inhibit

0x0255

598

0x02

R

BOOL N

Antibackspin inhibit

0x0256

599

Reserved

0x0257

600

0x02

R

BOOL N

Direction change inhibit

0x0258

601

0x02

R

BOOL N

Speed change inhibit

0x0259

602

0x02

R

BOOL N

Custom stop inhibit

0x025A

603

0x02

R

BOOL N

Firmware update inhibit

0x025B–0x025F

604–608

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?