DOCA0355EN-00

Communication Status

The table lists the communication status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x02A0

673

0x02

R

BOOL N

Modbus RTU or PROFIBUS DP port – No communication

0x02A1

674

0x02

R

BOOL N

HMI port – No communication

0x02A2–0x02BF

675–704

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?