Locked Rotor Protection
The table lists the locked rotor protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0DC4 |
3525 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DC5 |
3526 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
150–1000 |
200 |
Y |
Pickup |
|
0x0DC6 |
3527 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0DC7 |
3528 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
150–1000 |
200 |
Y |
Alarm level |
|
0x0DC8 |
3529 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DC9 |
3530 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto–Reset delay |