Voltage Imbalance Protection
The table lists the voltage imbalance protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E3D |
3646 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
3 |
Y |
Function setting |
|
0x0E3E |
3647 |
1 |
0x03, |
RW |
1 |
%Vn |
UINT16 |
5–50 |
10 |
Y |
Pickup |
|
0x0E3F |
3648 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0E40 |
3649 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
5–50 |
10 |
N |
Alarm level |
|
0x0E41 |
3650 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E42 |
3651 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E43 |
3652 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |