Communication Loss
The table lists the communication loss for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0EC8 |
3785 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
0x0EC9 |
3786 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
1–60000 |
10 |
Y |
Time delay |
0x0ECA |
3787 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0ECB |
3788 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0ECC |
3789 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Trip in remote mode only |