LTMTCT/LTMTCTV Sensor Module Device Internal Error Detection Setting
The table lists the different device Internal error detection setting for the LTMTCT/LTMTCTV sensor module Modbus RTU communication.
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
---|---|---|---|---|---|---|
0x0280 |
641 |
0x02 |
R |
BOOL | N |
Watchdog timeout detected |
0x0281 |
642 |
0x02 |
R |
BOOL | N |
ADC conversion error detected |
0x0282 |
643 |
0x02 |
R |
BOOL | N |
Flash error detected |
0x0283 |
644 |
– |
– |
– |
– |
Reserved |
0x0284 |
645 |
0x02 |
R |
BOOL | N |
Voltage configuration not detected |
0x0285 |
646 |
– |
– |
– |
– |
Reserved |
0x0286 |
647 |
0x02 |
R |
BOOL | N |
Calibration error detected |
0x0287 |
648 |
0x02 |
R |
BOOL | N |
VL1 measurement error detected |
0x0288 |
649 |
0x02 |
R |
BOOL | N |
VL2 measurement error detected |
0x0289 |
650 |
0x02 |
R |
BOOL | N |
VL3 measurement error detected |
0x028A |
651 |
0x02 |
R |
BOOL | N |
IL1 low gain measurement error detected |
0x028B |
652 |
0x02 |
R |
BOOL | N |
IL1 high gain measurement error detected |
0x028C |
653 |
0x02 |
R |
BOOL | N |
IL2 low gain measurement error detected |
0x028D |
654 |
0x02 |
R |
BOOL | N |
IL2 high gain measurement error detected |
0x028E |
655 |
0x02 |
R |
BOOL | N |
IL3 low gain measurement error detected |
0x028F |
656 |
0x02 |
R |
BOOL | N |
IL3 high gain measurement error detected |
0x0290–0x029F |
657–672 |
– |
– |
– |
– |
Reserved |