DOCA0355EN-00

Digital Input Interlock Protection Settings

Description

Each digital input interlock protection settings are made up of five registers. The order and the description of the settings for digital input 1 interlock are valid for the other digital inputs.

Address

Register

RW

Function code

Description

0x0F23–0x0F27

3876–3880

RW

0x03,0x06,0x10

Digital input 1 interlock protection settings

0x0F28–0x0F2C

3881–3885

RW

0x03,0x06,0x10

Digital input 2 interlock protection settings

0x0F2D–0x0F31

3886–3890

RW

0x03,0x06,0x10

Digital input 3 interlock protection settings

0x0F32–0x0F36

3891–3895

RW

0x03,0x06,0x10

Digital input 4 interlock protection settings

0x0F37–0x0F3B

3896–3900

RW

0x03,0x06,0x10

Digital input 5 interlock protection settings

0x0F3C–0x0F40

3901–3905

RW

0x03,0x06,0x10

Digital input 6 interlock protection settings

0x0F41–0x0F45

3906–3910

RW

0x03,0x06,0x10

Digital input 7 interlock protection settings

0x0F46–0x0F4A

3911–3915

RW

0x03,0x06,0x10

Digital input 8 interlock protection settings

0x0F4B–0x0F4F

3916–3920

RW

0x03,0x06,0x10

Digital input 9 interlock protection settings

0x0F50–0x0F54

3921–3925

RW

0x03,0x06,0x10

Digital input 10 interlock protection settings

0x0F55–0x0F59

3926–3930

RW

0x03,0x06,0x10

Digital input 11 interlock protection settings

0x0F5A–0x0F5E

3931–3935

RW

0x03,0x06,0x10

Digital input 12 interlock protection settings

Digital Input 1 Interlock Protection Settings

The table lists the registers for the digital input interlock protection settings.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0F23

3876

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0F24

3877

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–6000
(step 1)

0

Y

Time delay

0x0F25

3878

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0F26

3879

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–6000
(step 1)

0

Y

Auto-Reset delay

0x0F27

3880

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?