Wiring Diagram of LTMT Main Units Installed in an Enclosure
Overview
This section describes the connection of LTMT main units installed in an enclosure to the RS 485 bus via open-style connectors. Daisy chain connection is not possible when using the HMI port.
Precautions
Always follow the recommendations for wiring and connection.
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
This equipment must be installed, programmed, and serviced
only by qualified personnel.
Incorrect configuration can result in unpredictable behavior
of the devices.
Respect all the wiring and grounding rules in order to
avoid communication malfunctions due to EMC disturbance.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
LTMT Main Units Installed in an Enclosure
Installation Rules in a Switchboard
The installation of the LTMT main unit in the withdrawable drawer of a switchboard contains constraints specific to the type of switchboard:
-
For installation of the LTMT main unit in a Schneider Electric Okken switchboard, refer to the Okken Communications Cabling & Wiring Guide (available on request).
-
For installation of the LTMT main unit in a Schneider Electric BlokSeT switchboard, refer to the BlokSeT Communications Cabling & Wiring Guide (available on request).
-
For installation of the LTMT main unit in a Schneider Electric Model 6 switchboard, refer to the Model 6 Communications Cabling & Wiring Guide (available on request).
-
For installation of the LTMT main unit in other types of switchboard, follow the specific EMC instructions described in this guide and refer to the relative instructions specific to your type of switchboard.
Modbus RTU Accessories
The table lists the Modbus RTU accessories.
Designation |
Description |
Reference Number |
---|---|---|
Line terminator for open-style connector |
R = 120 Ω |
– |