DOCA0355EN-00

LTMT Main Unit Device Internal Error Detection Setting

The table lists the different device internal error detection setting of LTMT main unit.

Address

Register

Function code

RW

Type

Svd

Description

0x0260

609

0x02

R

BOOL N

Sensor module communication error detected

0x0261

610

0x02

R

BOOL N

Expansion unit communication error detected

0x0262

611

0x02

R

BOOL N

HMI communication error detected

0x0263

612

0x02

R

BOOL N

EEPROM interface error detected

0x0264

613

0x02

R

BOOL N

EEPROM checksum error detected

0x0265

614

0x02

R

BOOL N

Configuration error detected

0x0266

615

0x02

R

BOOL N

PROFIBUS DP interface error detected

0x0267

616

0x02

R

BOOL N

Internal temperature major error detected

0x0268

617

0x02

R

BOOL N

Watchdog timeout detected

0x0269

618

0x02

R

BOOL N

Low Battery detected

0x026A–0x026B

619–620

Reserved

0x026C

621

0x02

R

BOOL N

Energy register overflow

0x026D

622

0x02

R

BOOL N

Error detected during expansion unit initialization

0x026E

623

0x02

R

BOOL N

RTC initialization error detected

0x026F

624

0x02

R

BOOL N0

Internal temperature minor error detected

0x0270–0x027F

625–640

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?