Motor Stop Error Detection
The table lists the motor stop error detection for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0EBE |
3775 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
1 |
Y |
Function setting |
0x0EBF |
3776 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
1–60000 |
10 |
Y |
Time delay |
0x0EC0 |
3777 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0EC1 |
3778 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |