DOCA0355EN-00

Product Versions

The hardware versions of the TeSys Tera system are coded XXYY in UINT32 registers, with the following format:

  • Register 0: Reserved

  • Register 1:

    • XXYY: Hexa code of ASCII characters

Example: the LTMT main unit hardware version A is coded:

  • Register 9163 = 0x0000

  • Register 9164 = 0x0041

The firmware versions of the TeSys Tera system are coded aaa.bbb.ccc in UINT32 registers, with the following format:

  • Register 0: ccc, revision

  • Register 1:

    • MSB: aaa, major version

    • LSB: bbb, minor version

Example: the LTMT main unit firmware version 001.002.004 is coded:

  • Register 9165 = 0x0004

  • Register 9166 = 0x0102

Address

Register

No.

Function code

RW

Type

Svd

Description

0x23CA

9163

2

0x03

R

UINT32

Y

LTMT main unit hardware version

0x23CC

9165

2

0x03

R

UINT32

Y

LTMT main unit firmware version

0x23CE

9167

2

0x03

R

UINT32

Y

LTMT main unit boot firmware version

0x23D0

9169

2

0x03

R

UINT32

Y

LTMTCT/LTMTCTV sensor module hardware version

0x23D2

9171

2

0x03

R

UINT32

Y

LTMTCT/LTMTCTV sensor module firmware version

0x23D4

9173

2

0x03

R

UINT32

Y

LTMTCT/LTMTCTV sensor module boot firmware version

0x23D6

9175

2

0x03

R

UINT32

Y

LTMTCUF control operator unit hardware version

0x23D8

9177

2

0x03

R

UINT32

Y

LTMTCUF control operator unit firmware version

0x23DA

9179

2

0x03

R

UINT32

Y

LTMTCUF control operator unit boot firmware version

0x23DC

9181

2

0x03

R

UINT32

Y

LTMT expansion unit 1 hardware version

0x23DE

9183

2

0x03

R

UINT32

Y

LTMT expansion unit 1 firmware version

0x23E0

9185

2

0x03

R

UINT32

Y

LTMT expansion unit 1 boot firmware version

0x23E2

9187

2

0x03

R

UINT32

Y

LTMT expansion unit 2 hardware version

0x23E4

9189

2

0x03

R

UINT32

Y

LTMT expansion unit 2 firmware version

0x23E6

9191

2

0x03

R

UINT32

Y

LTMT expansion unit 2 boot firmware version

0x23E8

9193

2

0x03

R

UINT32

Y

LTMT expansion unit 3 hardware version

0x23EA

9195

2

0x03

R

UINT32

Y

LTMT expansion unit 3 firmware version

0x23EC

9197

2

0x03

R

UINT32

Y

LTMT expansion unit 3 boot firmware version

0x23EE

9199

2

0x03

R

UINT32

Y

LTMT expansion unit 4 hardware version

0x23F0

9201

2

0x03

R

UINT32

Y

LTMT expansion unit 4 firmware version

0x23F2

9203

2

0x03

R

UINT32

Y

LTMT expansion unit 4 boot firmware version

0x23F4

9205

2

0x03

R

UINT32

Y

LTMT expansion unit 5 hardware version

0x23F6

9207

2

0x03

R

UINT32

Y

LTMT expansion unit 5 firmware version

0x23F8

9209

2

0x03

R

UINT32

Y

LTMT expansion unit 5 boot firmware version

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?