Modbus RTU Network Characteristics
Overview
This section defines the characteristics of the Modbus RTU network over serial communication line. The Modbus RTU unit complies with the serial line specification. For information on serial line specification and implementation, see Serial Line Specification and Implementation Guide published on www.Modbus.org.
Standard Diagram
The standard diagram corresponds to the Modbus RTU specification on the www.Modbus.org site and in particular to the two-wire multidrop serial bus diagram.
Characteristics for Connection to Modbus RTU RS 485 Bus
The RS 485 standard allows variants with characteristics like:
-
Line terminator
-
Number of servers
-
Bus length
|
Characteristics |
Value |
|---|---|
|
Maximum number of stations (without repeater) |
32 stations, which is 31 servers |
|
Type of trunk cable |
Single, shielded, twisted pair cable, with 120 Ω characteristic impedance, and at least a third conductor |
|
Maximum bus length |
1000 m (3300 ft) at 19200 bps |
|
Maximum length of tap-offs |
|
|
Line terminator |
120 Ω resistor +/- 5% at both ends of the bus |
|
Common polarity |
Common polarity is connected to the protective ground in at least one point on the bus. |