DOCA0355EN-00

Trip Code

Trip code

Trip description

1

Thermal overload trip

2

Locked rotor trip

3

Stalled rotor trip

4

Definite time overcurrent trip

5

Normal inverse overcurrent trip

6

Short time overcurrent trip

7

Calculated ground trip

8

Measured ground trip

9

Phase under current trip

10

Current imbalance trip

11

Current phase loss trip

12

Current phase reversal trip

13

Phase under voltage trip

14

Phase over voltage trip

15

Voltage phase loss trip

16

Voltage imbalance trip

17

Voltage phase reversal trip

18

Under frequency trip

19

Over frequency trip

20

Excessive start time trip

21

Communication loss trip

22

Over Temperature trip

23

Under power trip

24

Over power trip

25

Under power factor trip

26

Reserved

27

Device internal trip

28

HMI communication loss trip

29

Wiring error detection trip

30-32

Reserved

33

Interlock 1 trip

34

Interlock 2 trip

35

Interlock 3 trip

36

Interlock 4 trip

37

Interlock 5 trip

38

Interlock 6 trip

39

Interlock 7 trip

40

Interlock 8 trip

41

Interlock 9 trip

42

Interlock 10 trip

43

Interlock 11 trip

44

Interlock 12 trip

45–48

Reserved

49

LTMT main unit temperature

50-94

Reserved

95

Stucked reset key

96

Logic test interrupted trip

97

Motor stop error detection trip

98

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?