DOCA0355EN-00

Protection Function Status

Protection Alarm Status

The table lists the protection alarm status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0100

257

0x02

R

BOOL N

Thermal overload alarm

0x0101

258

0x02

R

BOOL N

Locked rotor alarm

0x0102

259

0x02

R

BOOL N

Stalled rotor alarm

0x0103

260

0x02

R

BOOL N

Definite time overcurrent alarm

0x0104

261

0x02

R

BOOL N

Normal inverse overcurrent alarm

0x0105

262

0x02

R

BOOL N

Short time overcurrent alarm

0x0106

263

0x02

R

BOOL N

Calculated ground current alarm

0x0107

264

0x02

R

BOOL N

Measured ground current alarm

0x0108

265

0x02

R

BOOL N

Phase under current alarm

0x0109

266

0x02

R

BOOL N

Current imbalance alarm

0x010A

267

0x02

R

BOOL N

Current phase loss alarm

0x010B

268

0x02

R

BOOL N

Current phase reversal alarm

0x010C

269

0x02

R

BOOL N

Phase under voltage alarm

0x010D

270

0x02

R

BOOL N

Phase over voltage alarm

0x010E

271

0x02

R

BOOL N

Voltage phase loss alarm

0x010F

272

0x02

R

BOOL N

Voltage imbalance alarm

0x0110

273

0x02

R

BOOL N

Voltage phase reversal alarm

0x0111

274

0x02

R

BOOL N

Under frequency alarm

0x0112

275

0x02

R

BOOL N

Over frequency alarm

0x0113

276

0x02

R

BOOL N

Reserved

0x0114

277

0x02

R

BOOL N

Communication loss alarm

0x0115

278

0x02

R

BOOL N

Over temperature alarm

0x0116

279

0x02

R

BOOL N

Under power alarm

0x0117

280

0x02

R

BOOL N

Over power alarm

0x0118

281

0x02

R

BOOL N

Under power factor alarm

0x0119

282

Reserved

0x011A

283

0x02

R

BOOL N

Device internal temperature alarm

0x011B

284

0x02

R

BOOL N

HMI communication loss alarm

0x011C–0x011F

285–288

Reserved

Protection Pickup Status

The table lists the protection pickup status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0120

289

0x02

R

BOOL N

Thermal overload pickup

0x0121

290

0x02

R

BOOL N

Locked rotor pickup

0x0122

291

0x02

R

BOOL N

Stalled rotor pickup

0x0123

292

0x02

R

BOOL N

Definite time overcurrent pickup

0x0124

293

0x02

R

BOOL N

Normal inverse overcurrent pickup

0x0125

294

0x02

R

BOOL N

Short time overcurrent pickup

0x0126

295

0x02

R

BOOL N

Calculated ground current pickup

0x0127

296

0x02

R

BOOL N

Measured ground current pickup

0x0128

297

0x02

R

BOOL N

Phase under current pickup

0x0129

298

0x02

R

BOOL N

Current imbalance pickup

0x012A

299

0x02

R

BOOL N

Current phase loss pickup

0x012B

300

0x02

R

BOOL N

Current phase reversal pickup

0x012C

301

0x02

R

BOOL N

Phase under voltage pickup

0x012D

302

0x02

R

BOOL N

Phase over voltage pickup

0x012E

303

0x02

R

BOOL N

Voltage phase loss pickup

0x012F

304

0x02

R

BOOL N

Voltage imbalance pickup

0x0130

305

0x02

R

BOOL N

Voltage phase reversal pickup

0x0131

306

0x02

R

BOOL N

Under frequency pickup

0x0132

307

0x02

R

BOOL N

Over frequency pickup

0x0133

308

0x02

R

BOOL N

Excessive start time pickup

0x0134

309

0x02

R

BOOL N

Communication loss pickup

0x0135

310

0x02

R

BOOL N

Over temperature pickup

0x0136

311

0x02

R

BOOL N

Under power pickup

0x0137

312

0x02

R

BOOL N

Over power pickup

0x0138

313

0x02

R

BOOL N

Under power factor pickup

0x0139

314

Reserved

0x013A

315

0x02

R

BOOL N

Device internal pickup

0x013B

316

0x02

R

BOOL N

HMI communication loss pickup

0x013C–0x013F

317–320

Reserved

Protection Trip Status

The table lists the protection trip status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0140

321

0x02

R

BOOL N

Thermal overload trip

0x0141

322

0x02

R

BOOL N

Locked rotor trip

0x0142

323

0x02

R

BOOL N

Stalled rotor trip

0x0143

324

0x02

R

BOOL N

Definite time overcurrent trip

0x0144

325

0x02

R

BOOL N

Normal inverse overcurrent trip

0x0145

326

0x02

R

BOOL N

Short time overcurrent trip

0x0146

327

0x02

R

BOOL N

Calculated ground current trip

0x0147

328

0x02

R

BOOL N

Measured ground current trip

0x0148

329

0x02

R

BOOL N

Phase under current trip

0x0149

330

0x02

R

BOOL N

Current imbalance trip

0x014A

331

0x02

R

BOOL N

Current phase loss trip

0x014B

332

0x02

R

BOOL N

Current phase reversal trip

0x014C

333

0x02

R

BOOL N

Phase under voltage trip

0x014D

334

0x02

R

BOOL N

Phase over voltage trip

0x014E

335

0x02

R

BOOL N

Voltage phase loss trip

0x014F

336

0x02

R

BOOL N

Voltage imbalance trip

0x0150

337

0x02

R

BOOL N

Voltage phase reversal trip

0x0151

338

0x02

R

BOOL N

Under frequency trip

0x0152

339

0x02

R

BOOL N

Over frequency trip

0x0153

340

0x02

R

BOOL N

Excessive start time trip

0x0154

341

0x02

R

BOOL N

Communication loss trip

0x0155

342

0x02

R

BOOL N

Over temperature trip

0x0156

343

0x02

R

BOOL N

Under power trip

0x0157

344

0x02

R

BOOL N

Over power trip

0x0158

345

0x02

R

BOOL N

Under power factor trip

0x0159

346

Reserved

0x015A

347

0x02

R

BOOL N

Device internal trip

0x015B

348

0x02

R

BOOL N

HMI communication loss trip

0x015C–0x015F

349–352

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?