Stalled Rotor Protection
The table lists the stalled rotor protection for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0DBE |
3519 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
0x0DBF |
3520 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
50–1000 |
200 |
Y |
Pickup |
0x0DC0 |
3521 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
20 |
Y |
Time delay |
0x0DC1 |
3522 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
50–1000 |
200 |
Y |
Alarm level |
0x0DC2 |
3523 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0DC3 |
3524 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset Delay |