Last Motor Start Time Stamp
The table lists the last motor start time stamp for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|
0x15CA |
5579 |
1 |
0x03 |
R |
1 |
0 |
UINT16 |
Y |
Day |
0x15CB |
5580 |
1 |
0x03 |
R |
1 |
0 |
UINT16 |
Y |
Month |
0x15CC |
5581 |
1 |
0x03 |
R |
1 |
0 |
UINT16 |
Y |
Year |
0x15CD |
5582 |
1 |
0x03 |
R |
1 |
h |
UINT16 |
Y |
Hour |
0x15CE |
5583 |
1 |
0x03 |
R |
1 |
min |
UINT16 |
Y |
Minute |
0x15CF |
5584 |
1 |
0x03 |
R |
1 |
s |
UINT16 |
Y |
Second |
0x15D0 |
5585 |
1 |
– |
– |
– |
– |
– |
– |
Reserved |