Measured Ground Fault
The table lists the measured ground fault for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0DE7 |
3560 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
0x0DE8 |
3561 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
mA |
UINT16 |
20–20000 |
30 |
Y |
Pickup |
0x0DE9 |
3562 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
0x0DEA |
3563 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
mA |
UINT16 |
20–20000 |
30 |
Y |
Alarm level |
0x0DEB |
3564 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0DEC |
3565 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0DED |
3566 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
N |
Function while motor starting |