DOCA0355EN-00

Description

There are two ways to get the status data:

  • From BITMAP register, read with function code 0x03, where each register bit corresponds to one boolean data. For more information, refer to BITMAP Representation of Boolean Data.

  • From Boolean data, read with function code 0x02.

The table lists the status data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

Type

Svd

Description

0x15F9

5626

2

0x03

R

BITMAP

N

Digital Input Status.

0x15FB

5628

2

0x03

R

BITMAP

N

Digital Output Status.

0x15FD–0x1605

5630–5638

1

Reserved

0x1606

5639

1

Reserved

0x1607

5640

1

0x03

R

BITMAP

N

Common Trip, Alarm, and Pickup Status.

0x1608

5641

1

0x03

R

BITMAP

N

Motor Status.

0x1609

5642

2

0x03

R

BITMAP

N

Protection Alarm Status.

0x160B

5644

2

0x03

R

BITMAP

N

Protection Pickup Status.

0x160D

5646

2

0x03

R

BITMAP

N

Protection Trip Status.

0x160F

5648

1

0x03

R

BITMAP

N

Interlock Protection Alarm Status.

0x1610

5649

1

0x03

R

BITMAP

N

Interlock Protection Pickup Status.

0x1611

5650

1

0x03

R

BITMAP

N

Interlock Protection Trip Status.

0x1612–0x1617

5651–5656

1

Reserved

0x1618

5657 2

0x03

R

BITMAP

N

Starter Commands.

0x161A

5659 1

0x03

R

BITMAP

N

Motor Run Indicators.
0x161B 5660

2

0x03

R

BITMAP

N

Permissive Commands Status.

0x161D

5662 2

0x03

R

BITMAP

N

Inhibit Status.

0x161F

5664

2

0x03

R

BITMAP

N

LTMT Main Unit Device Internal Error Detection Setting.

0x1621

5666

2

0x03

R

BITMAP

N

LTMTCT/LTMTCTV Sensor Module Device Internal Error Detection Setting.

0x1622

5668

2

0x03

R

BITMAP

N

Communication Status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?