DOCA0355EN-00

Digital Input Settings

Description

The TeSys Tera system supports maximum 32 digital inputs:

  • Four digital inputs on the LTMT main unit.
  • Up to 28 digital inputs with LTMT expansion units.

Each digital input setting is made up of three registers. The order and the description of the settings for digital input 1 are valid for the other digital inputs.
Address Register No. Description DI location

0x1194

4501

3

Digital input 1 settings

DI1 on LTMT main unit

0x1197

4504

3

Digital input 2 settings

DI2 on LTMT main unit

0x119A

4507

3

Digital input 3 settings

DI3 on LTMT main unit

0x119D

4510

3

Digital input 4 settings

DI4 on LTMT main unit

0x11A0

4513

3

Digital input 5 settings

DI on LTMT expansion unit

0x11A3

4516

3

Digital input 6 settings

DI on LTMT expansion unit

0x11A6

4519

3

Digital input 7 settings

DI on LTMT expansion unit

0x11A9

4522

3

Digital input 8 settings

DI on LTMT expansion unit

0x11AC

4525

3

Digital input 9 settings

DI on LTMT expansion unit

0x11AF

4528

3

Digital input 10 settings

DI on LTMT expansion unit

0x11B2

4531

3

Digital input 11 settings

DI on LTMT expansion unit

0x11B5

4534

3

Digital input 12 settings

DI on LTMT expansion unit

0x11B8

4537

3

Digital input 13 settings

DI on LTMT expansion unit

0x11BB

4540

3

Digital input 14 settings

DI on LTMT expansion unit

0x11BE

4543

3

Digital input 15 settings

DI on LTMT expansion unit

0x11C1

4546

3

Digital input 16 settings

DI on LTMT expansion unit

0x11C4

4549

3

Digital input 17 settings

DI on LTMT expansion unit

0x11C7

4552

3

Digital input 18 settings

DI on LTMT expansion unit

0x11CA

4555

3

Digital input 19 settings

DI on LTMT expansion unit

0x11CD

4558

3

Digital input 20 settings

DI on LTMT expansion unit

0x11D0

4561

3

Digital input 21 settings

DI on LTMT expansion unit

0x11D3

4564

3

Digital input 22 settings

DI on LTMT expansion unit

0x11D6

4567

3

Digital input 23 settings

DI on LTMT expansion unit

0x11D9

4570

3

Digital input 24 settings

DI on LTMT expansion unit

0x11DC–0x11F1

4573–4594

3

Reserved

The settings of the four digital inputs on the LTMT main unit corresponds to the settings of digital input 1 to digital input 4.

The settings of digital inputs on a LTMT expansion unit are defined according to the expansion unit configuration.

Example: If the TeSys Tera system is composed of:

  • One LTMT main unit.

  • One LTMTIN42 expansion unit with four digital inputs, configured as expansion unit 1.

Then,

  • Digital input 1 settings to Digital input 4 settings are valid for DI1 to DI4 on the LTMT main unit.
  • Digital input 5 settings to Digital input 8 settings are valid for DI1 to DI4 on the LTMTIN42 expansion unit.

Digital Input 1 Settings

The table lists the registers for the digital input settings.

Address

Register

No.

Function code

RW

X Unit

Type

Range Default value

Svd

Description

0x1194 4501 1

0x03,
0x06,
0x10

RW

1

UINT16

0: Active high

1: Active low

0

Y

Digital input 1 trigger type

0x1195 4502 1

0x03,
0x06,
0x10

RW

1

UINT16

0–38
(step 1)

4

Y

Digital input 1 input source
0x1196 4503 1

0x03,
0x06,
0x10

RW

1 ms UINT16

1–60000
(step 10)

10

Y

Digital input 1 validation time

DI Input Source

The table lists the input source for the digital input settings.

Register value DI input source

0

Other

1

Trip Reset DI

2

Breaker Close DI

3

Breaker Open DI

4

Local-START> DI

5

Local-START>> DI

6

Local-STOP DI

7

Local-START< DI

8

Local-START<< DI

9

Remote-START> DI

10

Remote-START>> DI

11

Remote-STOP DI

12

Remote-START< DI

13

Remote-START<< DI

14

Interlock 1

15

Interlock 2

16

Interlock 3

17

Interlock 4

18

Interlock 5

19

Interlock 6

20

Interlock 7

21

Interlock 8

22

Interlock 9

23

Interlock 10

24

Interlock 11

25

Interlock 12

26

Contactor Open DI

27

Run DI

28

Block Input

29

Logic Test DI

30

Mode Selection 1

31

Mode Selection 2

32

Speed Change

33

Forced Start

34

Forced Stop

35

Self Test without Trip

36

Self Test with Trip

37

Reserved

38

None

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?