DOCA0355EN-00

Device Internal Status

The table lists the device internal status for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0EC4

3781

1

0x03,
0x06,
0x10

RW

0.1

Seconds

UINT16

1–60000
(step 1)

10

Y

Time delay

0x0EC5

3782

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication

3

Y

Reset mode

0x0EC6

3783

1

0x03,
0x06,
0x12

RW

0

UINT16

  • 0: Disable

  • 1: Enable

1

N

Internal temperature alarm

0x0EC6–0x0EC7

3783–3784

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?