Event Logs
Description
The last 100 events are recorded by the LTMT main unit. Each event log is composed of 8 registers.
A read request of 8xn registers is necessary to read n event logs, where 8 is the number of registers for each event log.
The order and the description of the registers for event log 1 are valid for the other event logs.
Address | Register | Description |
---|---|---|
0x1B58–0x1B5F | 7001–7008 | Event log 1 (most recent log) |
... | ... | ... |
0x1858–0x1B57 | 7001+8x(n-1) – 7008+8x(n-1) | Event log n |
... | ... | ... |
0x1E70–0x1E77 | 7793–7800 | Event log 100 |
Event Log 1 Registers
The table lists the registers for the event log 1.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|
0x1B58 | 7001 | 4 |
0x03 |
R |
– |
– |
UINT16 |
Y | |
0x1B5C | 7005 | 1 |
0x03 |
R |
– |
– |
UINT16 |
Y | Event Code |
0x1B5D | 7006 | 3 |
0x03 |
R |
– |
– |
UINT16 |
Y | Reserved |