DOCA0355EN-00

Extended Monitoring Data

The table lists the extended monitoring data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x16F3

5876

1

0x03

R

1

UINT16

N

Status word 1

0x16F4

5877

1

0x03

R

1

UINT16

N

Status word 2

0x16F5

5878

1

0x03

R

1

%IFLC

UINT16

N

L1 current (%IFLC)

0x16F6

5879

1

0x03

R

1

%IFLC

UINT16

N

L2 current (%IFLC)

0x16F7

5880

1

0x03

R

1

%IFLC

UINT16

N

L3 current (%IFLC)

0x16F8

5881

1

0x03

R

1

%IFLC

UINT16

N

Calculated ground fault (%IFLC)

0x16F9

5882

1

0x03

R

1

%IFLC

UINT16

N

Average current (%IFLC)

0x16FA

5883

1

0x03

R

1

%IFLC

UINT16

N

Maximum current (Imax)

0x16FB

5884

1

0x03

R

0.1

V

UINT16

N

For three phase, L1–L2 voltage

For single phase, L1–N voltage

0x16FC

5885

1

0x03

R

0.1

V

UINT16

N

L2–L3 voltage

0x16FD

5886

1

0x03

R

0.1

V

UINT16

N

L3–L1 voltage

0x16FE

5887

1

0x03

R

0.1

V

UINT16

N

Average voltage

0x16FF

5888

1

0x03

R

1

Hr

UINT16

N

Total RUN hour

0x1700

5889

1

0x03

R

1

Hr

UINT16

N

Last RUN hour

0x1701

5890

1

0x03

R

1

Sec

UINT16

N

Motor starting time

0x1702

5891

1

0x03

R

1

%IFLC

UINT16

N

Motor starting current (%IFLC)

0x1703

5892

1

0x03

R

1

KW

UINT16

N

Active power

0x1704

5893

1

0x03

R

1

KVAR

UINT16

N

Reactive power

0x1705

5894

1

0x03

R

1

KVA

UINT16

N

Apparent power

0x1706

5895

2

0x03

R

1

KWH

UINT32

N

Active energy

0x1708

5897

2

0x03

R

1

KVARh

UINT32

N

Reactive energy

0x170A

5899

2

0x03

R

1

KVAh

UINT32

N

Apparent energy

0x170C

5901

1

0x03

R

1

UINT16

N

Mode status

  • 0: Local1

  • 1: Remote

  • 2: Local2

  • 3: Local3

0x170D

5902

1

0x03

R

1

UINT16

N

Active trip count

0x170E

5903

1

0x03

R

1

UINT16

N

Active alarm count

0x170F

5904

1

0x03

R

1

UINT16

N

Trip code

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?