Definite Time Overcurrent Protection
The table lists the definite time overcurrent protection for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0DCA |
3531 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
0x0DCB |
3532 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
20–1000 |
110 |
Y |
Pickup |
0x0DCC |
3533 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
300 |
Y |
Time delay during motor start (TpS) |
0x0DCD |
3534 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
200 |
Y |
Time delay during motor run (TpR) |
0x0DCE |
3535 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
20–1000 |
110 |
Y |
Alarm level |
0x0DCF |
3536 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0DD0 |
3537 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0DD1 |
3538 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |