Current Imbalance Protection
The table lists the current imbalance protection for the Modbus RTU communication.
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
---|---|---|---|---|---|---|---|---|---|---|---|
0x0DF6 |
3575 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
3 |
Y |
Function setting |
0x0DF7 |
3576 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
% |
UINT16 |
5–100 |
20 |
Y |
Pickup |
0x0DF8 |
3577 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
50 |
Y |
Time delay |
0x0DF9 |
3578 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
5–100 |
20 |
Y |
Alarm level |
0x0DFA |
3579 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
0x0DFB |
3580 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
0x0DFC |
3581 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |