SUG_Wiser_China_WSE-06

E-mode LED behavior

Wiser AvatarOn devices have LEDs to indicate their operating status and to confirm actions such as resetting or joining a network.

Device

Status

LED indication

Duration

Wiser AvatarOn Smart Socket

Reset completed

Flash green

2 times

Wiser AvatarOn Freelocate (programming)

Programming mode On

Solid green

Until button pressed on freelocate to assign device controls/scene, or until programming mode time-out is reached

Wiser AvatarOn devices (control assignment)

Local control selected on device(s)

Local control backlight LED flashes

Until button pressed on freelocate to assign device controls

Local control(s) successfully assigned to freelocate button

Local control backlight LED flashes

5 times (freelocate LED also flashes green 5 times)

Wiser AvatarOn devices (E-mode scene programming)

E-mode scene successfully programmed to a button on freelocate

Flash green

5 times on freelocate and all programmed devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.