SUG_Wiser_China_WSE-06

Adding devices to the E-mode system

Join compatible Wiser AvatarOn devices and a freelocate remote controller to the E-mode system.
  • Make sure that the Zigbee network for the E-mode system has been created. (See Creating the network for E-mode.)

  • Remove the switch/dimmer fascia to access the controls on the switch/dimmer module. (See Supported Wiser devices for a link to the device installation instructions.)
  • If adding a freelocate, remove the freelocate from its metal bracket.
  1. Locate the Setup/Reset button on the device.
  2. Short press the Setup/Reset button 3 times.

The programming indicator LED on the device displays solid green.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.