SUG_Wiser_China_WSE-06

Programming the Advanced Feature buttons

The IR Convertor TV and HiFi control pages include 8 additional buttons that can be programmed with non-standard operations from the remote controller supplied with the appliance.

NOTE: You may need to tap the bar above the ADVANCED FEATURES label in order to access the button(s) for programming.

This example shows the TV control page. The Advanced Features section is identical in both the TV and HiFi control pages.

  1. (See A) Tap the Edit (pen) icon, then tap Learn.

  2. Tap the Advanced Feature button that you want to program.
  3. Follow the instruction in the dialog box to program the remote control function into the Advanced Feature button.

    NOTE: If the IR Convertor does not receive a signal from the remote control within 15 seconds, a Learning Failure message is displayed and the button is not programmed. Tap the Advanced Feature button for another 15 seconds of programming time.

  4. Repeat steps 2 and 3 to program the other Advanced Feature buttons.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.