SUG_Wiser_China_WSE-06

Setting Wiser Multifunction Interface channel communication parameters

Adjust the channel communication parameters on a Wiser Multifunction Interface to suit the make and model of thermostat(s) connected to that channel.
  1. Select the multifunction interface in the app.
  2. (See A, B) In the Multifunction Interface page, tap the Settings icon (A) and then select the channel to which the thermostat is connected (B).

    (Channel Multifunction1 is selected for this example.)

  3. Do one of the following:
    • (See C) Tap the Identify button to detect and set the required parameters automatically.
    • (See D) Manually adjust the parameters to suit the thermostat.
      TIP: Refer to Compatible thermostats for the Wiser Multifunction Interface to find the communication parameters for a specific thermostat make and model.
  4. (See E) Tap the Back arrow < to return to the Multifunction Interface page so that the thermostat can be added.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.