SUG_Wiser_China_WSE-06

Wiser IP Camera Indoor

Symptom

Possible cause

Solution

The Wiser IP Camera Indoor cannot connect to the internet via the Wi-Fi network router.

The router port settings may not be properly set for system access to the internet.

Check that the following router ports are open:

  • Port 6667

  • Port 6666

  • Port 6668

  • Port 6669

  • Port 1883

  • Port 8886

  • Port 8883

  • Port 443

IMPORTANT: For cyber-security, check that all unused ports are closed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.