SUG_Wiser_China_WSE-06

Resetting devices

Delete settings from a device, or remove a device from the system.
  • AvatarOn light switches, curtain switches and dimmers: Remove the switch/dimmer fascia to access the controls on the switch/dimmer module. (See Supported Wiser devices for a link to the device installation instructions.)
  • AvatarOn freelocate: Remove the freelocate from its metal bracket.
  • Wiser 360Degree ZB/IR convertor: The reset/eject tool is required.
  • Wiser smoke detector: Remove the smoke detector from its mounting bracket.

NOTE: After a device reset, all configuration data, user data, and network data is deleted.
  1. Locate the Setup/Reset/Function button and the programming/status LED on the device.
  2. All devices except Wiser multifunction interface: Press the Setup/Reset/Function button 3 times within 1 second and then press and hold the button for between 10 to 20 seconds.
    The programming/status LED flashes red.
  3. Wiser multifunction interface only: Press and hold the Clear button for at least 10 seconds.
    The Network Status LED flashes red.
  4. Release the button.

All devices except those specified below: The LED displays solid orange.

Battery-operated Wiser sensors only: The LED flashes green 7 times.

Wiser AvatarOn smart socket only: The LED flashes green 2 times.

All configuration, user and network data is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.