SUG_Wiser_China_WSE-06

Cuadro H Switches

ZigBee 1G Switch

This device is dedicated to switching the specified lighting load Or motor load (exhaust fan/motor) etc. The device can either pass Wiser by SE app or Smart Scene Switch, or use directly by pressing the local control key.

Instruction Sheet (PDF)

ZigBee 2G Switch

ZigBee 3G Switch

Zigbee 1G Curtain SW

Instruction Sheet (PDF)

Zigbee 2G Curtain SW

Instruction Sheet (PDF)

Zigbee 4K scene switch

After connecting to Wiser APP, it can be connected with other devices and equipped with scene control.

Instruction Sheet (PDF)

ZigBee 5P switch socket

The smart socket can provide a rated current output of 10A and can be connected to load not exceeding 2500W load.

Instruction Sheet (PDF)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.