SUG_Wiser_China_WSE-06

Light switches

Wiser AvatarOn 1G/2G/3G Switch

AvatarOn T switch 1G/2G/3G

Controls the lights in a room, or automatically switch lights On or Off in response to a specified condition or event.

AvatarOn 1G/2G/3G switch

AvatarOn T Switch 1G/2G/3G

Wiser 1 Gang Micro Module Switch

Converts compatible momentary switches into smart switches. Connect up to 10 compatible momentary switches .

NOTE: Momentary switches must be certified for use in 220–240 V AC applications.

Instruction Sheet (PDF)


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.