SUG_Wiser_China_WSE-06

About E-mode

Create a simple system that provides remote control for switching/dimming lights and opening, stopping and closing curtains.

This system is called E-mode and does not require a hub or the app. Instead, combine the Wiser AvatarOn series of light switches, curtain switches and dimmers to create a self-contained network of up to 30 devices. You can remotely control these devices using the Wiser AvatarOn Freelocate.

Configuration is achieved by operating the buttons on the devices. Moments can also be created using the freelocate.

NOTE: Do not set up an E-mode system where a Zigbee network created by a hub already exists.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.